12/18/2012 10:59 PM | |
Joined: 3/1/2012 Last visit: 10/2/2018 Posts: 1 Rating: (0) |
Hi, I'm trying to figure out if it is possible to create a ProfiNet-Network in ring-configuration which would allow two 414-5H CPUs to utilize the I/Os attached to that ring. The goal would be that the CPUs could both access the I/Os, regardless which CPU is currently operating as the Master. I have attached some views of a simplified sample configuration. Does anybody have any advice or hopefully some practical experience? Thank you! Hubert Attachment414-5H config 001.pdf (318 Downloads) |
12/19/2012 2:55 AM | |
Joined: 10/7/2005 Last visit: 5/2/2024 Posts: 3004 Rating: (1046)
|
Hello Hubert Reinartz even thoughI can't offer you any hands onexperience with this just yet, have a look the following info which should at least help with theconfig of a redundantPN based ET200M: Prerequisites (see also THIS link for more): ● CPU 41x-5H PN/DP as of version 6.0 ● IM 153-4BA00 as of version 4.0 ● STEP7 as of V5.5, SP2 HF1 |
Cheers |
|
Follow us on