1/15/2013 9:13 AM | |
Posts: 3 Rating: (0) |
thanks ... i want to sent analog data about 5km to controller.just siemens wifi is suitable for it ?? |
1/31/2013 5:52 PM | |
Posts: 2 Rating: (0) |
Take a look at the DATAEAGLE stuff.It is plug and play and we did not see any BUS errors. We connected our ET200M over a 2KM link working in 900MHz w/ LOS. They also have 2.4GHz and other freq. We worked with a company called M2M-Dynamics who installed it. http://www.m2m-dynamics.com/?page_id=519 We are also talking with them about a GSM/GPRS solution. |
2/1/2013 7:12 AM | |
Posts: 150 Rating: (17) |
Ubiquity hardware is very cheap and very reliable. We have used them in several occasions without any problems. |
Follow us on