4/26/2013 8:11 AM | |
Joined: 8/31/2010 Last visit: 5/15/2024 Posts: 1510 Rating: (222) |
Hello newbienew, refer this- Sample program: S7 communication GET and PUT instructions |
Like it? Rate it! |
|
4/26/2013 8:12 PM | |
Posts: 5 Rating: (0) |
Ethernet Communication: Data Exchange S7-1200 <-> S7-1200 (CE-X17) This is the sample of Siemens code I use However, I can set a bit to 1 and send out from Master in SLAVE that bit still 0 !! I dont know what did I do wrong so they dont communicate, please helpp !! |
Follow us on