6/3/2013 3:20 AM | |
Posts: 1 Rating: (0) |
Gents, I am trying to remotely connect to interrogate and modify the ladder pogram of a 317F-2 CPU from my office.I have a router and I have looked closely at the help document http://support.automation.siemens.com/WW/llisapi.dll/38571711?func=ll&objId=38571712&objAction=csView&nodeid0=10806083&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&load=treecontent we have set up our setting as per the example.Still can't get online "Partner not responding" I have set the "ethernet interface PN-IO" settings, which when directly connected is 192.168.0.XXX (being the CPU adrss)and changed itto the Router adress which is a 123.209.XX.XXX number and the subnet mask should be 255.0.0.0 (due to the 123 range). I can "ping" the router on 123.209etc and have set up the router to port forward the 192.168etc adress to port 102. the cable is connected to theport and the CPU and router are turned on. Any suggestions why I still cant connect??. Will I be able to modify the online program?? How does the program know to go out via the internet and not just the ethernet port?? Thanks in advance. |
Last edited by: SteveDel at: 6/3/2013 8:16 AM |
|
Follow us on