11/22/2005 11:26 AM | |
Joined: 8/31/2005 Last visit: 9/9/2025 Posts: 217 Rating:
|
Hello Leos! If you want to use the DEMO-connection to the SIMATIC NET OPC Server you have to activate the CP simulation. This CP simulation is a virtual communication device which is connected to a virtual PLC. Only with this CP simulation activated you have access to the simulated values of the OPC items shown in the scores7.txt file: [DEMO(Aliases)] DemoTemperature=DB10,INT12 DemoPower=DB10,DWORD14 DemoS7_DB=DB10,W0,6 DemoS7_E=EB0 DemoS7_A=AW0 [@LOCALSERVER(Aliases)] To activate the CP simulation just follow these steps (first close all OPC clients!):
|
Greetings, Chris |
|
This contribution was helpful to
1 thankful Users |
Follow us on