2/1/2014 8:38 PM | |
Posts: 784 Rating: (52) |
Hello Expert, Kindly find attached file. S7 communication between PC station and S7-1200 item ID:39960679.1-In page:20 IP address for OPC server:172.16.40.11 Subnet maskaddress :255.255.255.0 IP adress for CPU :172.16.43.20 I think the IP address for CPU would be 172.16.40.xxx not 172.16.43.20 2-In page:21 What is the meaning of "TSAP"? Best regards........ AttachmentSTEP 7 Professional V11_.pdf (34 Downloads) |
2/3/2014 10:06 AM | |
Posts: 1368 Rating: (126) |
Hello Eng.Mohammed, the ip addresses are correct, because the subnet mask is 255.255.0.0 This FAQ http://support.automation.siemens.com/WW/view/de/23586050describes the function of"TSAP" well. Greetings, Pittiplatsch |
This contribution was helpful to1 thankful Users |
Follow us on