10/16/2012 7:46 PM | |
Posts: 1 Rating: (0) |
Hi, I'm trying to read data from S7200 via CP-243-1 to 315-2PN/DP. I don't use CP 343-1 but Ethernet Interface integrated in s7300 CPU. I did everything (configured connections, IPs, TSAPs etc. in both PLCs) according to siemens manual ID 17369594: http://support.automation.siemens.co...ew/en/17369594 In S7300 in NetPro communication status is "Set up", S7200 shows that connection is ok. When I'm using "GET" function (FB14) in S7300 I'm always geting error code 1. Any ideas? Best Regards |
Last edited by: ptsd at: 10/16/2012 7:47 PM |
|
Follow us on