5/12/2014 4:31 PM | |
Posts: 65 Rating:
|
you can create wincc project in TIA Portal v12 or v13 on The PC at the first choose from HMI device configuration your HMI Panel type and the correct comunication method and create your project screens and download it to the HMI and after finishing take an archive that will be for your HMI then from HMI device configuration use PC general with the correct communication method and you will net simatic net to do that from the PC and choose your Screen resolution from Runtime settings general tab but you will have to adjust your all screens objects to fit the new screens resolution after finshing take an archive and that will be for your pc station |
Last edited by: ABDALKADER at: 5/12/2014 6:43 PMLast edited by: ABDALKADER at: 5/12/2014 4:37 PM |
|
5/28/2014 10:07 AM | |
Posts: 5 Rating:
|
First make a program for your HMI panel. After that you can create a WinCC PC System (SCADA). Make sure the resolution is correct for your PC screen. You can copy + paste your program from HMI into SCADA. Dont forget to copy the 'variables'. |
Follow us on