9/25/2014 11:19 AM | |
Posts: 3 Rating: (0) |
|
Last edited by: AutoGen_667188 at: 9/25/2014 1:04 PM |
|
9/26/2014 12:34 PM | |
Joined: 9/27/2006 Last visit: 7/11/2024 Posts: 12268 Rating: (2675) |
Hello Lütfen Okuyun; Even if many of us on the forum could understand Turkish, the amount of information you provide is ¸too small for us to understand your problem. At the very least, please tell us: - what CPU you are using; - what communication processor you will use; - what communication partner you need to exchange data with; - what protocol you want to implement, with details; is it straight ASCII, or Modbus ASCII, for example, and does it use special delimiting characters. In the meantime, please read the following information from Siemens Support, I hope it has a relation to the real question you have in mind: What properties, advantages and special features does the ASCII protocol offer? What should you watch out for when receiving data with ASCII drivers via serial S7-300/400 CPs? Hope this helps, Daniel Chartier |
This contribution was helpful to2 thankful Users |
Follow us on