11/12/2014 4:08 PM | |
Joined: 4/22/2010 Last visit: 5/3/2024 Posts: 5697 Rating: (713)
|
Hello, You don't have to add the module in Microwin, just connect it physically to the CPU The adressing depends on the CPU used, if you have one with buildin analog inputs (AIW0 and AIW2) the module adressstarts with AIW 4. If no onboard analog inputs it's AIW0 and further. Please have a look at S7-200 system manualfor more information, example is at page 48. Regards, Marcjan |
Last edited by: Marcjan at: 11/12/2014 4:11 PMProblem solved? |
|
11/14/2014 5:48 AM | |
Joined: 7/31/2014 Last visit: 1/29/2024 Posts: 11 Rating: (0) |
its done.thanks Marcjan. |
This contribution was helpful to1 thankful Users |
Follow us on