12/4/2014 7:48 AM | |
Posts: 21 Rating: (0) |
Dear sir, I m using PCS7.1 SP2 & CEMAT version 7.1 SP1.I have two server when server2 is master then all 6 client's operation is ok but when server1 is master then there is popup on all client "NO VALID LICENSE FOUND ON SERVER". Please find the attached screenshots of server1 licences & error pouop which comes on all clients. Please suggest.....
Attachmentlicenses.zip (131 Downloads) |
12/4/2014 9:56 AM | |
Posts: 32 Rating: (4) |
Hi, you say you're using CEMAT version 7.1 SP1 but why you're using a CEMAT Server Redundacy V6.1 License key then? It's maybe the wrong License on server1? You said when server2 is master all client's operations are working fine. Are you using the same License on server2 like on server1? By the way, you should have a look here: Siemens compatibility tool SIMATIC PCS 7 V7.1 SP2 isn't 'compatible' with CEMAT V7.1 SP1,in other words, it isn't approved by Siemens. |
Last edited by: Heisenberg_ at: 12/4/2014 9:57 AM |
|
12/18/2014 1:50 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
Follow us on