1/5/2015 7:13 AM | |
Joined: 12/29/2012 Last visit: 2/6/2024 Posts: 120 Rating: (15) |
Hi to all, Now i doing one project with S7200 with Panasonic Servo Drive. I wants to Control the Servo by pulse output from the the CPU224. I got one standard library from Siemens Website. In this library Homing Routine only Problem, remaing functions are working good. In that library, i used Q0.0 for pulse output and Reference point input I0.0. The problem is When i give the Home Execute command at the time the servo moved and it is not stopped even it hit the reference point switch . Please Help me to solve this issue. Here with i attched the program backup AttachmentMAP_SERV.zip (93 Downloads) |
Best regards |
|
Follow us on