2/2/2015 12:28 PM | |
Posts: 1 Rating: (0) |
Hello dear if i want to start the pump from button in HMI how can do that note i use wincc v6.0 and plc 300 s7
|
2/2/2015 2:46 PM | |
Joined: 3/14/2008 Last visit: 10/5/2024 Posts: 2107 Rating: (940) |
Lot of options, Easiest is a direct connection to a tag in S7, which starts the motor (In WinCC under the object Properties->Events->Mouse Click. |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on