4/3/2015 9:39 AM | |
Posts: 8946 Rating: (999) |
Is there a question? |
This contribution was helpful to1 thankful Users |
4/3/2015 10:45 AM | |
Joined: 5/20/2010 Last visit: 5/20/2024 Posts: 10 Rating: (0) |
addressing how to determine profibus? |
4/3/2015 3:49 PM | |
Joined: 1/28/2009 Last visit: 5/20/2024 Posts: 6840 Rating: (1359) |
Hello, If you want to select the PROFIBUS addresses of limit number of stations, there is an explanation of range and allowable numbers HERE.But if this has been configured , simply upload the whole station with STEP 7 and check the addresses assigned for each modules in hardware configuration.For ET200M, modular slaves, it is possible to check the slave addresses in form of DIP switches on the salve. I hope this helps, Hamid Hosseini |
Follow us on