4/3/2015 11:27 AM | |
Posts: 2 Rating: (0) |
Can a logo 8 connect directly to a PC, and if so is it with the provided Ethernet cable or does it need to be a cross over cable.
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 4/7/2015 1:11:47 PMNew súbject after splitting |
|
4/3/2015 11:58 AM | |
Posts: 2 Rating: (0) |
I want to connect directly to the logo with a pc without the use of a router I'm just wondering does this have to be a cross over cable |
Follow us on