10/26/2015 4:18 AM | |
Posts: 1 Rating: (0) |
Hi, Subject: Regarding Modbus TCP/IP Communication I'm using S7-1516-3PN/DP CPU and Siemens TIA Portal V13 Sp1 software for my application. My System is an intermediate among other systems. My system communication is through Modbus TCP with other / 3rd party system. I already made a Communication Setup, Using your sample program (Modbus Client and Server Configuration) . That helps me a lot. Now the Communication is estabilished between Server and Client. My requirement is to read 5000 Words (between 40001 to 49999) using Modbus Client (using same connection with server). Modbus Client, allows to fetch 125 Words per call. First 125 Words call are fetching, Remaining Call are getting Error. Regards, Vinoth R ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 10/26/2015 2:35:08 PMNew subject after splitting |
|
10/26/2015 4:59 PM | |
Posts: 3093 Rating: (323)
|
Hello Vinoth, Regards, |
10/27/2015 1:39 AM | |
Posts: 3 Rating: (0) |
Hi, Thank you for your swift reply. Error: 80A3 Regards, Vinoth |
11/5/2015 3:55 AM | |
Posts: 3 Rating: (0) |
Hi Javier, Do you mean one MB Server ID can communicate to Different MB Client ID? Is there any sample program available? Regards, Vinoth R |
Follow us on