4/13/2016 10:03 PM | |
Joined: 3/14/2008 Last visit: 9/26/2024 Posts: 2098 Rating: (938) |
Can you try to copy the contents of both images to your harddrive. Contents of disk 1 must be in folder named: "DVD_1" and contents of disk 2 in folder "DVD_2". Both in the same directory. And run the setup. Maybe there is a problem with the .mdx file... |
Last edited by: Oreca at: 4/13/2016 10:07:11 PMIf I could help you, you can use the RATE button. Thank you. |
|
4/13/2016 11:35 PM | |
Posts: 45 Rating: (0) |
Helle Oreca, Thank you for your reply , I did as you said but it doesn't work |
4/13/2016 11:37 PM | |
Posts: 45 Rating: (0) |
Dear Oreca, Thank you your answer. I did as you mentioned but it doesn't work for me |
4/13/2016 11:38 PM | |
Posts: 45 Rating: (0) |
this is the msg |
4/14/2016 9:18 AM | |
Joined: 3/14/2008 Last visit: 9/26/2024 Posts: 2098 Rating: (938) |
Or maybe because you unzipped the DVD's to an external disk? Anyway it looks like it. Can you try to use the C disk drive instead? Otherwise, I think there is something wrong with your .MDX file... |
If I could help you, you can use the RATE button. Thank you. |
|
4/14/2016 10:03 AM | |
Joined: 3/14/2008 Last visit: 9/26/2024 Posts: 2098 Rating: (938) |
You find me beautiful |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on