4/14/2016 11:06 AM | |
Joined: 10/31/2014 Last visit: 9/25/2024 Posts: 58 Rating: (5) |
hello, How to configured Scalance S602 Firewall Switch? |
4/14/2016 11:41 AM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
RIP |
Last edited by: 1test at: 6/8/2016 9:49:42 AM~(‾▿‾)~ |
|
4/15/2016 10:57 AM | |
Joined: 10/31/2014 Last visit: 9/25/2024 Posts: 58 Rating: (5) |
Can you describe the features of the data exchange in firewall? |
4/15/2016 12:31 PM | |
Joined: 11/21/2007 Last visit: 9/25/2024 Posts: 2325 Rating: (308)
|
Hello Pl have a look at this application example. Protection of an Automation Cell Using the SCALANCE S602 V3 and SCALANCE S623 Security Modules via a Firewall Also the following old threads will help you : Scalance S602 basics Problem with scalance S602 internal external IP set up Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
4/15/2016 12:45 PM | |
Joined: 10/31/2014 Last visit: 9/25/2024 Posts: 58 Rating: (5) |
Dear Navang, Thank You!!!!!!!! |
Follow us on