6/17/2016 9:19 AM | |
Posts: 567 Rating: (106) |
Hi Muneeb, it is not possible to Change the Name of the PC after installing and starting PCS 7 (WinCC). That has something to do with the SQL Server and Windows Groups for the SQL Server which were created during the Installation. Only way to Change the Name is new Installation of the PC station Have look at the this Manual entry. |
6/17/2016 4:32 PM | |
Posts: 567 Rating: (106) |
Did you only install PCS 7 again or also Windows? |
Follow us on