6/8/2010 7:48 PM | |||
Posts: 3 Rating: (0) |
For using FM350-2 counter module with PCS7 V7 I followed the entry
Parameter CFC(1).1.FM_DATA is not interconnected with a data source (block output, global address) In the other way when I wanted to generate Module Driver for it I received this warning message: (fig2,3) Cannot find driver block for the signal processing block 1 Thank you for your kind assistance. Attachmentpcs7 error.zip (64 Downloads) |
||
6/9/2010 7:12 AM | |
Posts: 3 Rating: (0) |
Hi
Thank you for your prompt assistance, First I bring your attention into these 2 files, both of them mentioned FM_DATA is interconnected automatically by compile or generating module driver, would you please guide me how can I connect it manually no usefull help is available for this pin.
Thanks & Regards
Attachmentfm350-2.zip (93 Downloads) |
6/10/2010 6:15 AM | |
Posts: 3 Rating: (0) |
Hi
I entered module address of this block but also face this error, please see the attachment.
In 2 computers I have installed PCS7 I see this problem.How can I access this structure(FM_DATA) in PCS7 is this relevant to DB which is required for using FM350-2 in S7 programs?
Thanks & regards.
Attachmenterror.zip (54 Downloads) |
10/6/2016 11:09 PM | |
Joined: 12/12/2013 Last visit: 5/22/2024 Posts: 31 Rating: (1) |
I am having this same issue. Has anyone solved it? |
Follow us on