8/9/2011 10:00 AM | |
Joined: 1/28/2009 Last visit: 10/26/2024 Posts: 6852 Rating: (1365) |
Hi What are the options for connecting a PG/PC online to the S7 controller via Ethernet? Regards |
8/11/2011 7:42 AM | |
Joined: 8/9/2011 Last visit: 9/10/2024 Posts: 12 Rating: (0) |
Thanks Leon, i have followed the document; https://support.automation.siemens.com/WW/llisapi.dll/19295355?func=ll&objId=21873792&objAction=csView&nodeid0=10806074&ehbid=19295355&query=pg+operation++CP343&lang=en&siteid=cseus&aktprim=0&extranet=standard&viewreg=WW&load=treecontent my PC IP configuration and comm.interface configuration are O.K. PLC : 192.168.5.222 Main PC:192.168.5.221 Router : 192.168.5.220 My PC: 192.168.5.229 i can send ping to all components above.i also disconnected the ethernet cable of main PC and assigned main PC address to mine and tried again.But i could not see the modules and CPU. Which kind of hardware configuration i need to see the CPU and modules? |
Follow us on