2/2/2017 11:14 AM | |
Joined: 3/14/2008 Last visit: 6/6/2024 Posts: 2070 Rating: (928)
|
Hi, What was the change that you made? Some changes cannot be done with download change. Can you follow the following FAQs? Is the host file correct? Can you see the OS computer on the ES and visaversa? Simatic Shell configured for the Terminal bus? (Check on ES+OS) Also listed at the top position? (Please check OS). The users and groups are setup correctly and equal on ES+OS? Can you check if the server package in WinCC Explorer is referring to the ES computer? |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on