10/9/2009 2:32 PM | |
Joined: 4/5/2006 Last visit: 10/10/2024 Posts: 917 Rating: (63) |
Hi razoh ,
I'm always a lil confused. When you say ArchiveManager folder in CAS station, do you means folder under WinCC project? If you means that, tht's wrong. You have to use "archive" folder from "network neigborhood": this is CAS share folder located somewhere depending of your installlation (CAS installation ask to you where you want create this folder)
just import OS Server Data in project station: - use simatic manager to create server data in OS CAS station (right click on the OS CAS and create server data - or - open OS CAS WinCC Explorer, right click on server data & create it. depend from your version) - import in OS Server & OS Client data server created in OS CAS (open OSs WinCC explorer, right click on server data and Load what created above) Anyway, try to import CAS OS Server data on the RunTime Wincc station (following procedure above).You should have 2 OS server data in the client station: form OS server & from OS CAS. Regards |
10/14/2009 5:04 PM | |
Joined: 4/5/2006 Last visit: 10/10/2024 Posts: 917 Rating: (63) |
Hi razoh, i dont't have CAS configuraton available on myPC right now, sorry ... ...but...yes, it should work. Lets know if will solve your trouble Regards |
3/20/2017 10:31 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4766 Rating: (122) |
New question published by meghna is split to a separate thread with the subject Not able to see Alarm data in the Alarm control data from the Process Historian. Best regards |
Follow us on