3/19/2017 6:46 PM | |
Posts: 5 Rating: (0) |
Hey Everyone, Step 7 Version : V5.5 + SP4 TIA Portal Step 7 : V13 SP1 Udpate 9 I am having a system which consist of CPU 414-5 H PN/DP with ET 200SP as decentralize periphery. I have CM PtP (6ES7 137-6AA00-0BA0) installed and to be used as MODBUS MASTER (RS485 2W) Following the given two links i proceeded with the programming, Required blocks were downloaded from this link: PtP communication instructions used on distributed I/O of an S7-300/400 Documentation: PtP instructions for use of ET 200MP / ET 200SP in the distributed peripherals of a S7-300/400 with Step 7 V5.5
Am I missing any update package ??? Or its just the way i made the blocks ??? For instance I have set a CPU 1510SP-1 PN with CM PtP (6ES7 137-6AA00-0BA0) installed as a SLAVE. I am attaching S7 Program for the Master ( Only the communication part ) Your Kind support is highly appreciated !!! AttachmentMASTER.zip (422 Downloads) |
Last edited by: Awel at: 3/19/2017 6:52:59 PM |
|
3/20/2017 10:56 AM | |
Joined: 2/27/2014 Last visit: 4/19/2024 Posts: 689 Rating: (199) |
Hello, Have a look in attached sample code. Use "Modview" Modbus RTU simulator testing software as Modbus RTU Slave. AttachmentModbus_1.zip (624 Downloads) |
With Best Regards, |
|
3/20/2017 2:15 PM | |
Posts: 5 Rating: (0) |
Hey, please find the attachment, Right now am trying to set the communication with MODBUS simulator, The thing is, At he moment the status of the FB Modbus Master shows always Buzy (7002) , without any successful done loop. Do I miss something in the assignment of the Modbus Master block or is it the way i initialize the Modbus Comm port FB640 ??! With Regards AttachmentSCREENSHOTS.zip (486 Downloads) |
Follow us on