10/14/2013 10:20 AM | |
Posts: 220 Rating:
|
Hi Chengyue, you can use for PCS 7 V7.0 and higher user defined FB from number 501. For the manuel and other PCS 7versions look here: http://support.automation.siemens.com/WW/view/en/2771491 To avoid conflicts I would start by FB2001 or just check the libraries you prefer to use and start by a higher number than in this libraries exsist. |
Last edited by: No Name at: 10/14/2013 10:33 AM |
|
10/18/2013 11:12 AM | |
Joined: 3/14/2008 Last visit: 8/3/2024 Posts: 2079 Rating:
|
With the addition of the new APL library, the range FB 0-2000 is reserved for the system. I prefer to start at FB2500 with you own custom blocks, as the libraries continue to being developed. You can also use DB's and FC's. The range for these is set in the "customize->compile/download" window, when you opened a CFC, under the options menu button. Standard, the range is set DB 1-60 and FC 60-700. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
2 thankful Users |
10/30/2013 1:52 PM | |
Posts: 567 Rating:
|
Hi, under the this FAQyou can find information how you can change existing FB numbers. Unfortunately the FAQ is only in german available. But there is an applicationavailable where the same topic is described in an example. You can find the example in chapter 6. |
7/18/2014 9:29 AM | |
Posts: 567 Rating:
|
Hi PackElend, you can find this information in the PCS 7 compendium part A chapter 7.1.2 "Creating user-defined technological blocks" http://support.automation.siemens.com/WW/view/en/63187279 |
7/18/2014 9:43 AM | |
Posts: 36 Rating:
|
thx |
3/28/2017 5:53 AM | |
Joined: 9/9/2015 Last visit: 7/29/2024 Posts: 727 Rating:
|
In my opinion, siemens should update the PCS 7 Power Control Library block reserved range in their Compendium Part A - Configuration Guidelines (V7.1/V8.0) , Guidelines on the range of numbers. The recomendation of user defined function block should be started with new range instead of FB2500 onward as it is occupied by Power Control Library. See attached with the Siemens function block guidelines. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on