3/28/2017 10:34 AM | |
Joined: 3/14/2008 Last visit: 5/27/2024 Posts: 2069 Rating: (928)
|
Hi, The symbol means that access protection has been enabled once and possible that Simatic Logon Role Management has been configured. This means that you can setup users and groups to enable/disable access to specific functions. If you select the subproject->Right Click->Access Protection and select: "Enable", then the symbol changes to red and it means the project is protected against changes and Role Management takes effect. To remove the icon, select "Enable" first and then select again the subproject->Right Click->Access Protection and choose: "Remove Access Protection and Change Log". This will remove the whole feature. You can access Role Management by choosing "Manage" in the submenu. |
Last edited by: Oreca at: 3/28/2017 10:37:08 AMIf I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to3 thankful Users |
Follow us on