5/1/2017 7:36 AM | |
Joined: 9/9/2015 Last visit: 5/21/2024 Posts: 727 Rating: (269) |
May be you could try these methods: 1. Use CUSTEPMAXRT 1. if you are using sfc type, assign a new input with data type "Time". This input will be your variable. Then set this input = with the CUSTEPMAXRT. (this method i have never used before, but you could try this out. ) 2. if method one failed, you can use CUSTEPRT (if there is only a few steps need such function) 1. Same with one, assign a new input with data type "Time", make a branch in the SFC, if the CUSTEPRT> the new input, go to another steps, Trigger process error. Hopefully the first method work for you. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
5/1/2017 8:05 AM | |
Posts: 62 Rating: (0) |
Thanks it is so helpful for me. |
5/1/2017 1:54 PM | |
Joined: 9/9/2015 Last visit: 5/21/2024 Posts: 727 Rating: (269) |
You are welcome. If I really solve your problem, please rate and close the thread, mark this thread as solved ya. Thank you. |
Last edited by: JazTai at: 5/1/2017 1:55:17 PMPlease give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
Follow us on