11/23/2017 4:56 PM | |
Posts: 1 Rating: (0) |
Hi there, I've somehow managed to establish VPN connection between S623 and M874-3 exactly as it is described in https://support.industry.siemens.com/cs/ww/en/view/99681225But use Scalance S623 instead Scalance S612 onlyScalance S623 is used how VPN Server Scalance M874-3 is used how VPN Client My Siemens Equipment is connected to internal port Scalance M874-3 via switch 1. My PC with control software is connected to internal port Scalance S623 I want to manage my siemens equipment. Therefore I shall to get access to M874-3 with my PC via VPN connection. My PC used IP address 192.168.2.26 mask 255.255.255.0 Internal port Scalance S623 used IP address 192.168.2.228 mask 255.255.255.0 Internal port Scalance M874-3 used IP address 192.168.3.179 mask 255.255.255.0 The PC1 connected to switch 1 used IP address 192.168.3.201 mask 255.255.255.0 The led for VPN connection status on the M874 is green. Therefore a VPN connection is established. Scalanace S623 and Scalance M874-3 used default firewall settings. But as I go on "Testing the Tunnel Function" I loking next results: From PC1 ping 192.168.2.228 is successfully From PC1 ping 192.168.2.26 is successfully From PC ping 192.168.3.179 is successfully From PC ping 192.168.3.201 is not successfully !!!! What this means ? It should be exactly that ? Where could be the problem? I am with Win7 and XP Windows on PC and PC1 Windows firewall on both PC is disabled. Thanks a lot an advance Best regards Vladimir |
Last edited by: Jen_Moderator at: 11/24/2017 11:10:05 AMInserted right link. |
|
Follow us on