12/11/2017 1:56 PM | |
Joined: 7/9/2015 Last visit: 7/25/2024 Posts: 3892 Rating: (571) |
Hi, if you use BSEND you can use Bool, Byte, Char, Word, Int, Real, Dint, Date, TOD, Time... Datatypes and there is nothing to set. Please check Output Parameter Status at you BSEND instruction. If Error get true (this could be only for one CPU cycle) save Status (this could be too fast for viewing). Also check this FAQ; How do you program communication blocks FB12 "BSEND" and FB13 "BRCV" for data exchange in the S7 program of an S7-300 CPU?Regards, Towome |
|
|
This contribution was helpful to1 thankful Users |
Follow us on