3/22/2016 11:40 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
Hello, Well, at this point, ESXi5.5 is released only for PCS7 8.1. See attachment. If you are really want to use it, I suggest you will get 5.5 version. Or maybe when PCS7 8.2 comes out (somewhere this year I hope), maybe ESXi 6.0 is supported. |
If I could help you, you can use the RATE button. Thank you. |
|
3/23/2016 10:43 PM | |
Posts: 1 Rating: (0) |
Greatings We have successfully installed and run a pair of Redundant PCS7 V8.1 OS Servers on VMware Vsphere 6.0. There are really not much tricky configuration about it, just make sure to check all the considerations about the things that you can and can't do. https://support.industry.siemens.com/cs/attachments/61630923/INH_SIM-NET_76.pdf |
Last edited by: Min_Moderator at: 3/24/2016 9:17:50 AMEdit links to permanent ones |
|
3/24/2016 9:26 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927) |
Yeah, Siemens did not test ESXi 6.0. Do you want to tell the customer that you want to use software, which is not yet released for 8.1? Good luck with that! Ofcourse it can work, but what problems will you get? And what if you have problems, Siemens will not help you because you need to install 5.5 |
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on