5/23/2018 10:00 AM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928)
|
Hi, I hope I understand your question: You want the block icons to have a specific layer like layer 5, but after generating the block icons, they are reset to 0? If so, you have to change the layer in the block icons in the "@PCS7TypicalsV8.pdl", not in the process pictures where they are inserted. If you have created a copy of this file like "@PCS7TypicalsV8_Custom.pdl" and the same icons are also in this file, the system will use the block icons in the _Custom, so you have to change the layer in that file.
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on