6/15/2018 3:21 PM | |
Joined: 9/27/2006 Last visit: 9/26/2024 Posts: 12283 Rating: (2685) |
Hello Boost; Open PCS 7 licenses are availabnle in conjunction with the purchase of certain Siemens industrial PCs (IPC), configured for a specific version of PCS 7 (v8.1 in your case, v8.2 and v9.0 are available at this time). You will have much information available in the following cattalog: https://www.automation.siemens.com/w2/efiles/pcs7/pdf/76/stpcs7_201415_catalog_en_Web.pdf IPC stands for one of the SIMATIC IPC types from the product range in the section "Industrial Workstation/IPC, Pre-configured bundles, SIMATIC Rack PC" which are authorized for SIMATIC PCS 7 V8.1. Section 10 is dedicated to OpenPCS 7, see the attached screenshot for explanations. Section 1 describes the available PCS 7 v8.1 IPCs, components and order numbers are analysed in section 3. Software bundles for OS are discussed in section 4, the licenses proposed include OpenPCS 7. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 6/15/2018 3:25:40 PM |
|
Follow us on