7/11/2018 6:43 AM | |
Joined: 10/24/2016 Last visit: 8/30/2024 Posts: 6 Rating: (0) |
hello my friends i have big problem in my system i have a system with two server and five client that one of server is standby .my servers use RAID hard . i use pcs7 7.1 sp3 in my system . suddenly on of server destroy that hang up i installed all of the software on it and downloaded my project . after restart system when system start up the problem repeat system wait on STATION CONFIGURATION EDITOR on 5% and hang up when i see the windows task manager there is many server running !!!! i attached picture are you any idea? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 7/11/2018 8:37:07 AMNew subject after splitting |
|
Follow us on