6/3/2019 4:37 PM | |
Posts: 5 Rating: (0) |
I am developing an application in LabVIEW for a Test equipment which has the SIemens ET200AL Profinet gateway and there are two AI and DI modules linked to it. My requirement is to read the Analog and Digital sensor data and do something based on same. The real problem is to get the data from the Profinet bus and read them in Labview. For this the options are very limited as there is one PCI card from Kunbus PCI Profinet -Labview card But sadly the support from that company is lacking. SO I was wondering if there is a way I can access the Profinet bus data by a serial card if I buy a Siemens PLC system. Then I can simply read the data via a serial port. I don't need Real TIme performance and once every 50ms sampling is fine. Any ideas for a suitable hardware ?? Thanks |
Follow us on