9/18/2019 3:54 PM | |
Posts: 5 Rating: (0) |
Hi Why have Siemens opted to implement a unidirectional process for the OPC UA client? This adds a lot of work to mapp variables back and forth in the PLC program, for conventional OPC UA communication it is possible to subscribe to a variable that is read/write enabled and both read it and write it. I can't find any explanation to why the implementation isn't bidirectional. You should be able to use the same "list" to read and write and have a single point for the data. Do you have any input on this? Regards Marcus ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 09/19/2019 07:25:18New subject after splitting |
|
9/20/2019 9:00 AM | |
Posts: 5 Rating: (0) |
Hi This thread was split from a previous one so thats why I didn't specify products. But yes, I mean the OPC UA client in S7-1500 and TIA portal v15.1 |
Follow us on