(0)| 11/7/2019 11:39 AM | |
|
Joined: 11/30/2016 Last visit: 12/6/2022 Posts: 1 Rating:
|
I have s7 414 4h PLC with 2MB flash memory card, PLC in rack1 is working fine but PLC in rack -0 all LED's flashing so we replaced CPU of rack 0 with CPU of same version of firmware and same order number. We downloaded the program in memory card but when we download the program in CPU memory it is giving error of insufficient memory.We uploaded the blocks from Rack -1 CPU and downloading the same in Rack 0 CPU same error. 1.My question is if same program is running in Rack 1 why we are not able run the same program in rack -0. 2.Rack 0 PLC is not coming Run MOde.Stop LED is constant. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/07/2019 12:43:44New subject after splitting |
|
Follow us on