11/15/2019 10:15 AM | |
Joined: 10/2/2018 Last visit: 2/15/2023 Posts: 8 Rating:
|
Hi all, I currently have to integrate four EH Picomag meters to an S7-1200 1214C using the IO-Link (6ES7 278-4BD32-0XB0). As I was having difficulty with the PCT tool and there seems to be a memory limitation of 32bytes ( and I need to use all four ports with 120bits per device), I have opted to use the IO-link function block available. In the attached snippet, you will see my logic with the block. Every four seconds I send a request to have a look at the parameters of the flow meters. However, I currently receive exactly the same data in the DB with every request. I am somewhat lost here. Also, I have checked but cannot find the correct IOL_Index to use with these picomag meters. Please advise on this. Morever, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/15/2019 11:17:33New subject after splitting |
|
11/15/2019 11:51 AM | |
Joined: 6/19/2017 Last visit: 8/5/2024 Posts: 8175 Rating:
|
|
My Forum is the place to personalize your profile, |
|
Follow us on