12/20/2012 8:19 AM | |
Joined: 9/6/2008 Last visit: 5/7/2022 Posts: 1121 Rating: (86) |
Hi Well go thourgh the link and go to technical tab and see the links. LInk1 Have fun... |
Jazz |
|
12/21/2012 12:56 PM | |
Posts: 9 Rating: (0) |
Yes,I had already seen this docs but there is no information about my issues. :-( Thanks Anyway. |
12/21/2012 2:22 PM | |
Posts: 836 Rating: (99)
|
Hi, do you know the Siemens Industry Mall where you can order products? You can also find marketing information to those products, check out the infos of yours (click on product information): https://eb.automation.siemens.com/mall/en/DE/Catalog/Products/10041907 Maybe it helps. |
Last edited by: Silent Bob at: 12/21/2012 2:23 PM |
|
1/1/2013 8:19 PM | |
Posts: 836 Rating: (99)
|
Hi, sorry, I really don't know about that. |
9/1/2013 4:12 PM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello thidalgo,proinelcapower I will try to answer your questions to the extent i know. a) Licensing : The Licensing is in the form of a Registration code which is linked to the MMC Serial No. ( For CPU with MMCs )or CPU Serial No ( for CPUs withou MMC ). You can buy Ready Bundles which Include the Hardware + Software + Registration Codes. Various Bundle combinations are available to suit all requirement. Alternatively you can just by the software libraries and request for the Registration codes by provding your Licence Details and the MMC / CPU Serial No of MMC / CPU already available with you. b) Multiple Masters : Multiple Masters are allowed - by using -By using Cascading Function - Normally used for multiple links to same control centre. -By implementing the thecomplete IEC chain multiple times. I do not think SIPLUS RIC Blocks impose any restriction on this. The Limitations applicable would depend upon the CPU processing capability andmax. no of TCP/IP connections possible. ( Two TCP/IPPorts are reserved for each call of FC 100 ) c) No of SIgnal Points : §SIPLUS RIC Bundles with SIMATIC S7-400H for up to 5000 information points Buffer Size 3200 Information points §SIPLUS RIC Bundles with SIMATIC S7-400 For up to 5000 information points Buffer Size 3200 Information points §SIPLUS RIC Bundles with SIMATIC S7-300 For up to 2000 information points Buffer Size 800 Information points §SIPLUS RIC Bundles with SIMATIC ET 200S For up to 200 information points Buffer Size 800 Information points You can raise a specific request to SIPLUS RIC Support at siplus-ric.automation@siemens.com for any clarifications. Hope this helps Cheers Navnag |
There is no such thing as the last bug in a program |
|
Follow us on