11/6/2018 1:36 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi Janko, Strange problem on a new installation.. Can you restart and try again creating a project with PCS7 wizard, but now without any OS objects: No PCS7 OS, no OpenPCS7 OS, no Simatic Batch and no route control? **If you haven't did this already** When it succeeds, try to add a new subproject with PC station-> with WinCC Application (server project). Can you upload the diagnose files as well-> Under C:\Program Files(x86)\SIEMENS\WinCC\diagnose. Thx |
If I could help you, you can use the RATE button. Thank you. |
|
11/27/2018 10:06 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hi Kandishishi, it seems that the problem with the wizard is a bigger problem. With regards |
2/25/2019 7:44 PM | |
Joined: 2/1/2010 Last visit: 4/26/2024 Posts: 134 Rating: (68) |
HI all, I did have this problem in one of my projects. I installed the TH update (and actually all updates) from the 9.0 SP1 product page and my problems were resolved. Link to updates: https://support.industry.siemens.com/cs/document/109756832/ Hopefully it works for you. |
If my post helped you, please rate. Thanks. |
|
This contribution was helpful to1 thankful Users |
12/13/2019 9:39 PM | |
Posts: 1 Rating: (0) |
Hello, I opened the link you gave above and what i found was PCS7 Engineering System Collection V9.0 SP2 (EU/ASIA) (1,2 GB) , should i download and install it? |
12/13/2019 10:22 PM | |
Joined: 2/1/2010 Last visit: 4/26/2024 Posts: 134 Rating: (68) |
Specific to just the hierarchy issue with PCS7 9.0 SP1 as title of this post, I suggest Engineering Collection SP2 on the ES (and you will need to update SFC on your OS and clients to be in step) as well as TH V9.0 SP1 Upd1 at a minimum, but you should evaluate to install the other relevant system components in section 4 of the updates page as well. In more general terms, just my advise, not official procedure: When you are installing a brand new system, install all the updates (all of them to the relevant PCs, not just the Engineering Collection to ES). Use Thunderstorm's pinned post. If you are in production, and are having a problem, install the updates and take note of consequences/restrictions. If you are in production and not having a problem, don't install the updates until your next maintenance interval according to your site plan. |
If my post helped you, please rate. Thanks. |
|
This contribution was helpful to1 thankful Users |
Follow us on