1/8/2020 12:26 PM | |
Joined: 11/29/2011 Last visit: 5/7/2024 Posts: 1358 Rating: (231) |
Hi, I have to do exactly the same. See the attached picture for reference. The ES on site having an WinCC Appl. configured in the ES configuration. I suppose I need remove this and reconfigure a Wincc Appl. Client Ref. I have to implement this on a live system I need to be very quick. Is the compendium A is good enough to follow or is there something else to watch out for? ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 01/09/2020 19:35:50New subject after splitting - What you read here, please check with manuals and your requirements. |
|
1/9/2020 9:55 PM | |
Joined: 6/23/2008 Last visit: 5/4/2024 Posts: 1165 Rating: (279)
|
Hello MicroMan, I'm not 100% sure, but I think on an ES a referenced client is not possible (because it won't be downloaded to somewhere). Add a WinCC Apl. Client instead. Detailed information should be given here. Best regards... |
"Expert" does not necessarily mean Siemens employee. Please cross-check your requirements always with official Siemens documentation. Also "Experts" are pleased about feedback. Please don't send support requests as PM. Questioners who don't follow up their thread will be put to my list of users to be ignored. |
|
1/10/2020 4:27 AM | |
Joined: 9/9/2015 Last visit: 5/10/2024 Posts: 727 Rating: (268) |
Hello MicroMan, The way you configured in the ES is the way I learnt from Siemens Intensive Workshop. The purpose of configured ES with WinCC Application and removing the "OS" is because of realizing the WinCC OS Simulation function. With the WinCC Application configured, you can configure the same S7 Connection with the same name that OS Server A and Server B. Normally we configure the same s7 connection name for Server A and B to have the same tags. Now you can configure the same connection name for OS simulation. As what mark said, OS client refence in ES is not possible. You can create WinCC appl client instead.
|
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on