1/15/2020 9:10 PM | |
Posts: 1 Rating: (0) |
Hi I have a polygon drawing in wincc a motor and I want to make this drawing change colors by an integar tag For example Working green Stopped normal Alarm flashing red I have tried by moving 1 2 values to a memory word mw4 for example and make this memory word my tag but it doesn't work If any one can help pls ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 01/16/2020 08:50:50New subject after splitting |
|
1/16/2020 9:32 AM | |
Joined: 12/27/2018 Last visit: 7/19/2024 Posts: 510 Rating: (43) |
This worked for me.I made a logic like fault-yellow, alarm-red and healthy-green. You need to move an integer to an integer data type(eg:%md55). In HMI, Animation section select colors an flashing then select range for colors Assign numbers 1=red 2=green browse select tag from plc program.I Also you need to use move command 1 to int data type when motor on. similarly 2=off. Take care interlock in plc program if you handle more than 2 integers to HMI. It will work. otherwise test whether the output inter is coming to HMI by adding an io field adding this int data type in connection .then on motor you can see the tag value in iofield. |
Jinson Kurian Vilayil James, P.Eng, BE, M.Tech (Power Electronics and Power System),PGDM, MBA |
|
Follow us on