9/25/2019 8:09 AM | |
Joined: 8/21/2019 Last visit: 1/11/2023 Posts: 1 Rating: (0) |
Hi everyone, I configured S7-1200 PLC (192.168.0.2) as Modbus server, I'm using Modscan as a client(192.168.0.31). Server status showing 7002. I able to ping PLC from the PC, but if i try to connect modscan it showing TCP/IP terminated. I added a firewall in/out rules also. I am unable to find, where I'm making mistake. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 09/25/2019 10:04:05New subject after splitting |
|
This contribution was helpful to1 thankful Users |
5/5/2020 10:01 PM | |
Posts: 1 Rating: (0) |
Was this ever solved? I'm having the same issue.
|
Follow us on