7/3/2020 10:44 PM | |
Joined: 3/14/2008 Last visit: 11/9/2024 Posts: 2124 Rating: (951)
|
Hi, When you open the AP library in Simatic Manager, you can go to Templates folder and in there are a lot of examples of process tag types. You will find what you are looking for. Also take a look at the PCS7 Complete Overview page where examples are listed as well under tab: Advanced Process Control. See link. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
7/6/2020 7:32 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hi svbodhe, in the application example Equipment Modules for SIMATIC PCS 7 using the example of the Chemical Industry you can find some templates for different types of control loops and all control loops has an integrated simulation. There you also get some detailed information about the realization in PCS 7. With regards |
This contribution was helpful to2 thankful Users |
Follow us on