11/4/2008 10:41 PM | |
Posts: 2661 Rating:
|
Hi, Yes, this is possible. You can create FBD/STL blocks in PCS7 and you program String_0 & String_1 for IN_OUT BOOL parameters. See attachment. Regards Attachmentfbd_strings.pdf (218 Downloads) |
1/3/2009 7:22 AM | |
Posts: 261 Rating:
|
Hi PeVi, The String_0 and String_1 are reflected as "text reference” tag. The Start value is linked with the text library with ID. You can not change the Start Value normally (Tag which is generated by AS-OS compilation). You can generate the Text in text library and give the start value to tag by VBA.The code is shown. regards ddg Attachmentcode.pdf (210 Downloads) |
Follow us on