3/21/2019 3:48 PM | |
Joined: 11/29/2013 Last visit: 5/21/2024 Posts: 98 Rating: (3) |
Hi! WinCC Flex is 2008 SP5 (last version, I believe). Windows 10 is version 1709, build 16299.967. |
8/19/2021 10:49 AM | |
Joined: 12/19/2017 Last visit: 6/14/2024 Posts: 1 Rating: (0) |
Hi, I had this problem with TIA portal v16 running on windows 10 on a virtual machine (VMware). I managed to solve it by doing the following: - Host PC, set IPv4 adress to an IP in the scope of the device you want to connect to. In my case a PLC. Disable IPv6 protocol. - Host PC, disable all other network adaptors other than ethernet (not sure this is neccesary) - Host PC, download PRONETA (Trial version PRONETA Professional V1.1. - ID: 109781284 - Industry Support Siemens) - VMware, Set the VM network setting to bridged + replicate physical network. - VMware, make sure the VM can access PRONETA, I made a shared folder from my host PC mapped to a network drive in the VM. - VMware, start the VM - VM, If not already installed then install Siemens TIA portal and transfer licenses. - VM, go to change adaptor settings -> right click the ethernet adaptor -> select properties: - VM, now I had the problem of the empty PG/PC Interface list in the "Set PG/PC Interface" app in control panel and could not connect to my PLC. - VM, make sure you can ping the device you want to connect to. - VM, to fix the empty PG/PC list I ran PRONETA as administrator in the VM -> IO Test -> PRONETA scans the network and finds your device -> click on it -> click in the "IO Test" tab in the top of the screen. - VM, after the installation restart the VM and when booting up again the PG/PC interfaces are available in the "Set PG/PC Interface" app in control panel. *1, It might work by just running PRONETA folder/Misc/PC-IDENTIFYER/PC_IDENTIFYER.exe Voila :) |
Last edited by: ErikS.N. at: 08/19/2021 11:11:25Last edited by: ErikS.N. at: 08/19/2021 11:12:10Last edited by: ErikS.N. at: 08/19/2021 11:13:03Last edited by: ErikS.N. at: 08/19/2021 11:14:03Last edited by: Jen_Moderator at: 08/19/2021 11:16:34Optimized link. |
|
This contribution was helpful to1 thankful Users |
Follow us on