6/2/2021 8:17 AM | |
Posts: 198 Rating: (60) |
Hello, I am not sure if i understood your question right, however, if you are looking to create excel reports from the Information server, , the Information Server Office add-ins must be installed on the PC. This component must be selected during installation. In the license perspective, connection with the Information Server via Microsoft Excel, Word or PowerPoint will need the Information Server client access license. You can check the procedure for installation in section 1.3.3 of the manual linked here. https://support.industry.siemens.com/cs/ww/en/view/109766850 Hope this helps |
Last edited by: TechnoBlaze at: 06/02/2021 08:18:43Last edited by: TechnoBlaze at: 06/02/2021 08:19:07Last edited by: Jen_Moderator at: 06/02/2021 09:57:26Optimized link. |
|
This contribution was helpful to1 thankful Users |
10/8/2024 6:35 AM | |
Joined: 7/30/2024 Last visit: 10/8/2024 Posts: 193 Rating: (3) |
New question published by Rez98 is split to a separate thread with the subject Daily report keeps spitting the same Data. Best regards |
Follow us on