6/2/2020 12:00 AM | |
Joined: 3/14/2008 Last visit: 5/24/2024 Posts: 2069 Rating: (928)
|
Hi, There are only minimal requirements to the processor. With the i7 8/9th generation your good The only requirement is that you use a compatible OS. The following operating systems are supported in PCS 7 V9.0 incl. SP1: ● Windows 7 Professional SP1 (64-Bit, only English Windows language version) ● Windows 7 Ultimate / Enterprise SP1 (32-Bit) ● Windows 7 Ultimate / Enterprise SP1 (64-Bit) ● Windows 10 Enterprise 2015 LTSB (64-Bit) ● Windows Server 2012 R2 Standard Edition (64-Bit) (as "Windows Server 2012 R2 Standard with Update" or incl. KB 2919355 „Windows Server 2012 R2 Update“) ● Windows Server 2016 Standard Edition (64-Bit) P.S: It might be cheaper in the end to buy pre-installed PCS7 systems. They are called Siemens IPC and you can configure them yourself like adding redundant power supply, choosing from a set of processors, with or without CP1623 card, memory, hard disks etc. They come pre-installed, so you only have to fill in the Computer name. PCS7 is already installed (except licenses of course;) ) |
Last edited by: Oreca at: 06/02/2020 00:04:55If I could help you, you can use the RATE button. Thank you. |
|
6/2/2020 10:55 AM | |
Joined: 3/14/2008 Last visit: 5/24/2024 Posts: 2069 Rating: (928)
|
Glad to help! Good luck! |
If I could help you, you can use the RATE button. Thank you. |
|