6/28/2013 2:11 PM | |
Posts: 62 Rating:
|
Dear AZR, Please check the Plant hirerarchy sittings,derive block_icon,creat&updateblock icon setting. increat&update block icon setting change the lower hirererchy setting as per the project hirerachy level. For more details please find attached file. Regards, Avinashkrishna Bhimavarapu
AttachmentPlant hierarchy.zip (190 Downloads) |
This contribution was helpful to
1 thankful Users |
6/28/2013 3:18 PM | |
Joined: 6/8/2013 Last visit: 8/5/2024 Posts: 188 Rating:
|
hi i checked the sections you say but problem is not solved.. im tired.... |
6/28/2013 4:12 PM | |
Posts: 691 Rating:
|
Dear a.z.r Can you please check the Block Properties Settings of the Block called in the CFC. Check the OCM Possible and Create Block Icon Options in the Block Properties.At the WinCC end, Open the @PCS7_Typicals.Pdl in the Graphics Designer and check the Block Icon Number of the desired Block Icon. Make the Create Block Icon Number to 1 in the Chart and then compile the OS . Check whether the Block Icons are created are not Also upload the Block Properties Screen shot |
Last edited by: Niranjan Prasad at: 6/28/2013 4:30 PM |
|
This contribution was helpful to
1 thankful Users |
6/1/2014 6:28 PM | |
Joined: 8/1/2012 Last visit: 9/2/2024 Posts: 179 Rating:
|
Hi Thanks for reply. I do the procedure with another PC (PCS7 V7.1) and the result is OK . there must be a problem in libraries and faceplates Wish the best for king of Automation Mo.Sa AttachmentDesktop.zip (172 Downloads) |
|
|
Follow us on