1/26/2024 8:05 PM | |
Joined: 6/11/2019 Last visit: 5/11/2024 Posts: 2194 Rating: (98) |
A program often says more than a thousand words. I have added a message text to my example ptogram and adapted your LWE project to my program. But note that the button for switching between manual and random consists of two elements ! On the one hand, a button with transparent images and no text, which is queried by the logo program with NI11. On the other hand, there is a status display with text and images directly underneath, which is controlled via NQ1. The analog network input NAI2 queries the position of the slider.Take a look at the settings in the LWE.I assigned the address VW10 to the slider. greeting Ella_68 AttachmentProgrammplan-2b-LWE.zip (151 Downloads) |
Follow us on