4/13/2011 2:42 AM | |
Posts: 2661 Rating: (279)
|
Does your custom block creates EventState (alarms)? See the following: How should I configure a message block (FB43) so that it can be linked with a group display? |
This contribution was helpful to1 thankful Users |
5/8/2011 7:21 AM | |
Posts: 88 Rating: (0) |
Hiiiii, How did u solve? pls suggest,,,, Regards, Manoranjan |
5/8/2011 9:37 AM | |
Posts: 2661 Rating: (279)
|
Check the bits in the EventState variable. See Fig 01 in the following FAQ: How can you have alarms displayed in the process picture with the smart object "Group Display" when the bit alarm procedure or analog alarm is being used as the alarm process? Also see the following FAQ: What can you do if no messages are displayed in the overview area of WinCC? Regards |
This contribution was helpful to2 thankful Users |
Follow us on